This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS22995H-Q1: On-Resistance

Part Number: TPS22995H-Q1

Hello,

the maximum on-resistance is specified for VBIAS = 3.3 V, VIN = 3.3 V and IOUT = -200 mA with 29 mOhm for the temperature range -40..125 °C.

Please specify the maximum on-resistance for currrents up to -3 A.

Thanks in advance.

Best regards,

Alexander