I am looking for a 12V, 1A regulated supply from 12-100V input. I used this reference design and tested the circuit on a breadboard with THT resistors and capacitors.
The output resistor is 1k ohm and I am getting linear output till 20V. It damaged chips on higher voltages.
What could be the problem?
"I am searching for a regulated power supply that provides 12V and 1A, and can take input within the range of 12-100V. I have used a reference design and constructed a circuit on a breadboard using through-hole resistors and capacitors. The output resistor is 1k ohm and I am getting a linear output until 20V. However, when I try to increase the voltage beyond 20V, the chips get damaged. Can you help me identify the problem?"