This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LP5860: Is this the right driver

Part Number: LP5860


Hello

I have a design requirement where I need to drive 198 bidirectional leds. The LED forward voltage in one direction is 2.0V and in the direction is 1.4V, the current is 20mA. My question is

1) Is there a way to use the LP5860 to drive the LED

2) Is there another device that i should use.