This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2980:BQ298019RUGR

Part Number: BQ2980

Hello expert 

I want to set ;

under voltage:2.5V

over voltage:4.2V

I want to charge the li-ion battery up to 4.2V and turn it off when the battery voltage is 4.2. I want to turn off the load when the battery voltage is 2.5v. Which values should I play with?

thank you 

best regards