Dear Team,
Could you help to review the schematic as below?


Many Thanks,
Jimmy
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
HI Jimmy,
Here are some comments:
1. The EN pin pull-up resistance should be smaller(20k) because the internal pull-down resistor can be 225-900k.
2. It's better to add a 5Ω resistor in series with Cboot to reduce SW spike. Too high spike at SW node might cause device damage.
Regards,
Shipeng
Hi Shipeng,
EN Voltage
Ven = 12V*( R269 // Ren(225k) / ( (R269//Ren(225k) ) + R268) = 2.7V > 1.6V


Many Thanks,
Jimmy
Hi Jimmy,
For U12, there's pull-down resistor so the situation would be better. Your calculation is right, and if it's 900k, the EN voltage is 2.96V.
For the 5Ω resistor, I can say that's related to your layout. If customer has used this device before and there's no issue happens, they can keep their layout and ignore this resistor. Otherwise, this resistor should be put in for backup.
Thanks.
Shipeng
Hi Shipeng,
Thus the EN resistance of U12 can be keep the current design, right?
The resistor you want has been reserved footprint in the Cboot side, attached the latest schematic and layout, please help to review and give your advices. I have sent the file over mail. Thanks for your great support.
Many Thanks,
Jimmy