Hello:
The customer is using LM5148 for a power supply that converts 48V to 33V, with a continuous current of 2A. Currently, they are encountering two issues:
1. No output voltage, no matter how the input voltage is adjusted, there is no output
2. Static power consumption is particularly high, reaching 15mA without load
At the request of the customer, it is not convenient to place the schematic and PCB layout on the forum. Please provide a private email to help check and provide some solutions. Thank you!!!