Other Parts Discussed in Thread: TPS65993,
Hi, we're planning to use the TPS65994AERSLR in a new design and are preparing the code for the microcontroller that will be loading the TPS65994AERSLR's config file via I2C.
The TPS65993_4 Application Customization 6.4.31 Tool offers export of binary, hex and c config files.
Can you confirm that the Patch Bundle for just the "Low Region (TPS6599x)" address region is the correct payload that our MCU should transmit over I2C to configure the TPS65994AE upon each startup?
We could not get the TI tool to generate a C file output when selecting the "Full flash image (TPS6599x)" option.
Regarding the flow chart in Figure 5-1 of SLVUC38, in the "Write Patch Bundle burst data..." step, should the Header ID word of 0xACE00001 be included in the data transmitted to the PD controller?
We are not using an EEPROM.
Thank you.