Hi,
Some questions for the LED current tolerance and would like to check with BU.
1. According to datasheet, the first line spec in captured below is around 10% tolerance and the 2nd line is +3.4% ~ -3.2%.
They are all in 20.2mA LED current, so this is confusing me what is exactly tolerance spec.
Please help to clarify.

2. My customer application will use exponential mapping control and the brightness will be less than 2014brightness code.
That means the LED current is very low for the brightness requirement of <1nits brightness backlight lighting.
Could you please provide the low brightness tolerance spec to me (brightness code between 0 to 1024 at full scale= 20mA)?

3. If LM3697 is not suitable for low LED current (6uA) application, please help to suggest alternative part.
Thanks and Best regards,
Tiger