Other Parts Discussed in Thread: TPS631010
Hi,
We plan to use the TPS63901 in a space constrained design. In the worst case its power input can be as low as 3.8 V while it outputs 5 V.
On the datasheet plot (Figure 8-4) the current with an input of 3.6 V is specified up to 0.7 A.
Could you please confirm that it can supply a 0.7 A continuous current with an input voltage as low as 3.8 V and an output of 5 V ?
Many thanks in advance for your help.