hi, we're using BQ25798 to charge 3S Li-Ion battery pack using 12V HVDCP. IC works with 1uH inductor, 1A charging limit and 1.5 MHz switching frequency. We did notice acoustic noise and wrong ADC readouts when the Power Stage switches from buck to boost operation towards the end of charge (Uusb ~11.6 V, Ubat = 12.45V, Ibatt <0.3A) Disabling PFM in forward mode solves the issue. The issue is not present in BQ25798EVM. Can it be due to too high MLCC capacitors used on PMID and SYS causing unstable loop operation? If yes are there max recommended values?
BQ25798EVM:
- PMID: 3x10uF (C2012X5R1E106K125AB) = 3x1.67uF@12.5V = 5uF@12.5V + 33uF tantal
- SYS: 5x10uF (C2012X5R1E106K125AB) = 5x1.67uF@12.5V = 8.35uF@12.5V
- BATT: 2x10uF (GRT188R61E106ME13D) = 2x1.5uF@12.5V = 3uF@12.5V
Our board
- PMID: 3x22uF (C3225X7R1E226M250AB) = 3x14.8uF@12.5V = 44.4uF@12.5V
- SYS: 3x22uF (C3225X7R1E226M250AB) = 3x14.8uF@12.5V = 44.4uF@12.5V
- BATT: 2x22uF (C3225X7R1E226M250AB) = 2x14.8uF@12.5V = 29.6uF@12.5V
additionally our board has similar issues in buck mode when working with 2.2uH inductor and 1.5MHz