Other Parts Discussed in Thread: BQ76942
My design consists of a 10S li-ion battery pack. The power distribution is seperated between the top 5 cells and the bottom 5 cells. The discharge is uneven between the top and bottom, with the top discharging at double the rate of the bottom.
This results in low battery cutoff by the top, when the bottom still has ~50% charge left. At this point, the battery is disconnected from the "tool"
I would like to use the BQ77915 for balancing during the charge cycle. If CC/CV charging is done at 1A, then the lower 5 cells will achieve full charge before the top, and therefore balancing is needed to bypass the "entire" charge current for the bottom cells while the top cells continue to charge.
Is my thinking correct here?
Thanks for any assistance!