This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM74502H-Q1: Turn on requirements

Part Number: LM74502H-Q1

I'm using a 74502H in a back to back mosfet switching application to connect inverters to batteries. VS is typically 50-56V.

I have the EN at 3V, so it should be enabled, but I am not seeing the 12V differential voltage across VCAP, and the src and gate pins are both low.

Pins 2 and 7 are grounded - no OV is used.

How do I get the charge pump to turn on?