Part Number: REF6041
Other Parts Discussed in Thread: ADS8881, REF70, REF54, TINA-TI
Hi,
I'm considering using REF6041 to replace my VREF + OP combination, 'cause the built-in buffer of the former. From the 'Load Regulation' specification I calculated that the output impedance in worst case is about 123 mOhm and the typical value only 8 mOhm. But the 'Output Impedance' specification states the typical value is 50 mOhm.
Why there is so big difference between the typical value calculated from 'load regulation' and the 'Output Impedance' specification? Which one should I use in my signal chain calculations?
Regards.