This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PMP23340UCD: CCS Compilation Environment Configuration

Part Number: PMP23340UCD
Other Parts Discussed in Thread: UCD3138A, UCD3138

HI guys,I encountered a problem when configuring the compilation environment.

  • Environment:Code Composer Studio 12.5.0(Compiler version [TI V5.2.9])
  • Part number:PMP23340UCD    (UCD3138A)
  • Firmware1:UCD3138_IBC_Firmware.(This Firmware is developed for UCD3138A device and for the IBC application and LLC topology.)
  • Firmware2:UCD Training-labs.

  • When I import the project(Firmware1), I find the configuration parameters as shown in the picture, is this correct?

  • I changed the chip number.But there was an error.

  • I tried to fix the above error and a new warning appeared, now what should I do.

  • I tried to replace the  CMD file but I get the same error.

  • But when I import another routine (Firmware2)and change the chip model and cmd file as above, there is no error.

Why is this, is this the right thing to do, and how do I fix this?!!Thank you.