This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61379-Q1: Inductance value

Genius 17675 points

Part Number: TPS61379-Q1

Hello,

My customer would like to use 10uH inductance in thier design and are seeing TPS61379-Q1 as one of candidates.
Table 9-2 in the datasheet shows 0.45 ~ 1uH for recommended inductors.
Can 10uH be used for this device?

Regards,
Oba

  • Hi Oba,

    What's the switching frequency and the mode that customer uses?

    Regards

    Lei

  • Hello Lei,

    They don't still have any idea for both switching frequency and the mode.
    They just want to reuse 10uH that is already on their AVL.

    Regards,
    Oba

  • Hi Oba,

    Here are the two general rules to judge whether 10μH can be used for TPS61379:

    • If it works in PFM mode, the inductor ripple should be bigger than 800mA;
    • If it works in PWM mode, 10μH should work, but it's better to check that the right-half-plane zero is still at least 5 times bigger then the crossover frequency. The TPS61378 calculation can be used for TPS61379.  

    Once customer provides more detailed work conditions, I can also take the more careful check.

    Regards

    Lei