Other Parts Discussed in Thread: TPS54160, TPS54260
hello,
i have a problem with TPS54160 EN pin.
In some devices i have observed a different behavior with the same circuit interface (R1-R2 from page 14 of datasheet).
Input parameters:
VI = 5V
Vout = 3.3V
VSTART = 4,75V
VSTOP = 4,20V
R1 = 180K
R2 = 64,9K
The circuit works always correctly, but some devices have a VSTART higher than other so the output is not generated.
The En threshold has a large range and is variable with temperature..
But i watched that with decreasing value of resistence R1-R2 (in same ratio) the circuit is always activated.
There is a minimum current in input for EN pin?
There is a graphic more complete of VEN vs VIN and Temperature (fig 9 page 8)?
Thanks in advance
Davide