This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM5117-Q1: Absolute Maximum Ratings of LM5117-Q1

Part Number: LM5117-Q1


Dear team,

I understand that if even a momentary surge is applied to Vin that exceeds the absolute maximum rating, may potentially breaking the device and affect its reliability.
But, I would like to confirm the following as the customer's request.

・Is there a possibility that the Gate Driver circuit will be broken by surges exceeding the maximum rating on VIN?
・Additionally, is there a possibility of device breaking even if the maximum rated voltage is exceeded for a few microseconds?

Best Regards,
Shingo