Dear TI experts,
My customer is looking for a DCDC buck module(integrated inductor) for their new project.
The requirement is as below;
input voltage : 5V ~ 21V
output voltage : 5V
output current : maximum 2A
the problem is minimum input voltage. they want to make 5V output even input voltage is 5V.
Could you recommend the module which meet this requirement?
Best regards,
Chase