Other Parts Discussed in Thread: UCC28781-Q1, UCC28C50-Q1, UCC28782, UCC28781, UCC28730
Hey TI Team,
I hope you are doing well. I needed your recommendation on using UCC28730-Q1 for DC-DC applications such that it meets the below-given specifications. Efficiency as well as quiescent current are the key parameters in my design. The quiescent current I'm aiming for is around 500uA at no load condition, which from the datasheet, I think is possible as the standby power of the device is around 5mW (Correct me if I'm wrong). I'm evaluating 2 TI ICs for the DC-DC converter: one is the UCC28730-Q1 and another is the UCC28781-Q1. I want to use this thread for my understanding of using UCC 28730-Q1 or UCC28781-Q1 to meet the below-mentioned specs.
| Flyback Converter Specifications | |||||
|
Sr. No. |
Parameter | Min | Typ | Max | Units |
| 1 | Input voltage | 60 | 100 | 150 | V |
| 2 | Output voltage | 12.5 | 13 | 13.5 | V |
| 3 | Power | 30 | W | ||
| 4 | Current | 2.2 | 2.3 | 2.4 | A |
| 5 | Efficiency | > 85 | % | ||
| 6 | Isolation | 3 | kV | ||
Note: I was previously using UCC28C50-Q1 (PSR feedback) to meet the above specs, but the design with UCC28C50-Q1 had very poor output regulation at no load, and the quiescent current was also around ~6mA.
What parameter should I change in the calculator of UCC28730 and UCC28782 (in place of UCC28781) to use it as a DC-DC controller. Currently, when I set the frequency to 0 (for UCC28730), a few cells of the recommended value show errors. If you have a DC-DC calculator for the same, can you please share it with me?
Regards,