Hi,
On our new designed board we are using 3 tps7a8300rgr devices.
2 of them are suppling 3.3 volt using ANY-OUT programmable outputs and are working fine.
another one is set to 1.8 Volt output using ANY-OUT programmable outputs but is failing to set the output level correctly.
the output level is stuck at 1.97 Volt (tried using the any out 50mV pin to adjust the output voltage levels differently but it doesn't seem to have any effect, the output level is stuck).
the problem reoccurred on another board.
the power supply schematic is as follows:
please suggest a way to proceed with this matter
Regards,
Lev