This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS6594-Q1: Solution to replace SC33PF8200 for J3 platform

Part Number: TPS6594-Q1

Hi Team,

Could you help suggest best solution to replace SC33PF8200  which showed in page 7 of https://www.nxp.com/docs/en/application-note/AN13863.pdf 

Thank you!

Marc

  • Hello Marc,

    This is possible, but there are more high current power supplies than a single TPS6594 can provide, but with an additional device it's possible.

    The 5A line would need to be supplied by a dual phase on the PMIC or have a separate high current power supply (BUCK).

    To continue this discussion, please post on the internal forums! :)

    BR,

    Nicholas