This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

LM25141-Q1: EMI issue

Part Number: LM25141-Q1


Hi,

Currently customers are using LM25141Q
There is a phenomenon of EMC exceeding the standard of 30M~108M
Check the datasheet, it is said that the Slew rate can be adjusted to reduce EMI.


Is there any recommended value for adjusting the slew rate?

Thanks &best regards,

  • Hello David,

    Slew rate can we adjust by adding a boot resistor in series with the boot capacitor.  You can also experiment with an RC snubber on the Switch node to ground.  Start with a ~1ohm 1206 resistor and a 100pF capacitor.  Can increase Capacitor to 470pf in gradual steps to tune out noise.

    Other things to try is a 100MHz ferrite bead on the input.  If these do not work, suggest a CM choke for higher frequency attenuation of CM noise.

    Hope this helps.

    David.