Due to TPS7A2020PYCKR Body Marking is Black rather than White, see below package image captured by our AOI. Our AOI is unable to read the Body Marking. If to adjust the Body Marking image matching setting up to 60% in AOI, it would cause some false calls. This would lead to AOI unable to detect if wrong polarity occurs. Is it possible to make the Body Marking color more brighter and visible to be readable by AOI?