Other Parts Discussed in Thread: BQSTUDIO,
Hi all,
We have selected this part for the one of our applications.
And we are using this rechargeable battery https://thinkrobotics.com/products/16340-battery-3-7v-1300mah?variant=39334535266390
And i have initializing the fuel gauge with following configuration.
1. chemical ID : 0x1202 (4.2V)
2. Design capacity (700mAh)
3. Design Energy (2.59 Wh)
And I am continuously reading the remaining capacity for every ten seconds.
Issues:
1. I am getting constant remaining capacity value even when I applied some load. But after the power on reset I am getting reduced capacity value.
Eg: I am getting 615 mAh value continuously even when I applied some load. But after the power on reset, the remaining capacity value reduced to 600 mAh.
2. When charging this battery, remaining capacity value getting reduced. But after the power on reset, the remaining capacity value increased.
Eg: when charging this battery, remaining capacity value getting reduced from 615 mAh. But after the power on reset, the remaining capacity value increased to 630 mAh.
Please provide the suggestion.
Regards,
Aslam