This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TLV61046A:Does not stabilize output with input less than 3,0V

Part Number: TLV61046A

My project uses this boost to raise 3.8v to 12V. This 12v feeds an RF transmitter with an average current of 20mA. I need it to supply 12v with an input above 1.8V.
The boost is not enough to keep the 12v stable at the output, look at the image (input voltage of 2.0V):

Meu projeto ultiza este boost para elevar 3,8v para 12V. Esse 12v alimenta um transmissor RF com corrente media de 20mA. Preciso que ele forneça 12v com entrada acima de 1,8V.

O boost não da conta de manter os 12v estável na saída, observe a imagem(tensão de entrada de 2,0V):

3.0V input voltage:

3.8V input voltage:

Peak current output is approximately 40mA.

Output current averages 20mA.

The effect happens on the EVM-TLV61046A and on my board too..

Project: