Hi,
The problem is the tripping of the OCC regardless settings in the protection. This happens only at values higher 2500mA (the default is 12000) . At values lower than 2500mA all works fine exact on the threshold of settings the safety alert is triggered. But at settings higher than 2500mA the threshold stucks at 2500mA although higher threshold values are set. How can that be? What could be the workaround for that.
THX in advance for proposals