Hi,
We set RIMON= 5.36kohm 1%, RSET= 100ohm 1%, RSNS=0.5mohm 1%. According the the equation from the datasheet, IMON=24.1mV when ILOAD=1A; IMON=241mV when Iload=10A.
The maximum value of IMON won't exceed 248mV when ILOAD=10A, considering all tolerance.
Equation:


Calculation:

However, the measured values don‘t like that. What could be the reason?If needed, I can send the SCH privately.