This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

PTH08T240W: Output current problem

Part Number: PTH08T240W


Hi team,

When use 12V input, 5V output, the output current can only reach 1A. They need about 10A output current. Could you help to solve this problem? Thanks.

Below is the schematic:

  • Hi Yang

    1. Change R2 to 0ohm and R7 to 0ohm

    2. if customer using turbo trans pls calculate the correct value for R5 by including Cout derating,

    looking at the Cout the cap value is wrong with respect to R5 value 10kohm

    3. track pin have internal RC circuit it is okay to use 0ohms at R3

    4. if smart sync is not used, it is recommended to connect smartsync pin to gnd.

    what is happening to the stability and vout after more current is drawn

    Thank you

    Savith