Hi,
I'm encountering an issue with the TPS65941111EVM. The only physical action I've taken is connecting VSYS. When attempting to enable any buck output via quick-start with VSYS connected to 3.3V using the stock NVM, I don't observe any voltage. However, when I use 5V, there is no such issue. The LDO output always works fine.
Buck output also worked fine when I conducted another test where I started with VSYS at 3.8V and then gradually reduced the voltage to 3.3V before attempting to turn on the buck output.
However, when I reversed the process, starting at 3.3V and then increasing to 3.8V, the issue persisted.
I'm uncertain if this behavior is normal. What's particularly concerning is the SPMI_ERR_INT, which only occurs when VSYS is lower than 3.8V."