This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS61252: VOut should be 3V3, but it's the same as VIn

Part Number: TPS61252
Other Parts Discussed in Thread: TPS63900

This is the first time I connect the circuit. I started using 3V6 and the VOut is the same as the VIn. When the VIn is below 3V3, the VOut remains at 3V3.
The measurement was made with the processor without firmware running. So the usage current is very low.
There is a key that will make EN equal to VIn. The processor starts and sets a pin high, keeping the tps enabled.
As there is no way to disconnect the VOut from the circuit, I am afraid of connecting the battery and damaging another component.
The total current when everything is working will be around 300mA
Would the fact that the current is very low cause this problem?
I used the datasheet specifications. Below is the schematic and part of the PCB. L1 is a Abracon 1R5

  • Hi Fernando,

    Boost is a kind of step up topology that only works when its output is higher than Vin. If you need both step up(when Vbat is 3V6) and step down(when Vbat is low), we recommend using Buck-Boost devices like TPS63900 orTPS63901.

    Best Regards,

    Travis