Dear Mr. Mrs.
About BQ79606 FMEDA calculate tool, we have some questions need your help:
- “Life Cycle” in <Mission Profile Tailoring>. Our project’s life cycle is very special, it need 15 years but active operating time is 27550 hours. So does the life cycle in the FMEDA tool can be modified according to our requirements?
- The operational profile in <Mission Profile Tailoring> is based on IEC/TR 62380, can you provide a SN29500 version?
- Whether this FMEDA calculate tool only for cell voltage monitoring and temperature monitoring, i.e. SG1 and SG2. If we want to calculate the FMEDA for SG3 and SG4, i.e. Cell Voltage Protection and Temperature Protection., Do we need to use a new FMEDA calculate tool?
- About <Pin Level Tailoring> in the FMEDA calculate tool, we just need to select whether the corresponding failure mode of every Pin is safety related or not, i.e Column G? Do we need to select the corresponding safety mechanism, i.e Column N? because in this table, the corresponding safety mechanism has been selected. If we want to select a another safety mechanism for a specific failure mode, Do we need to analyze the applicability and coverage of this mechanism?
- About <Function and Diag Tailoring> in the FMEDA calculate tool. We are not very clear about the effect of sub-circuit block's failure mode for Safety Goal or chip level system function. Does TI has some document or materials to introduce these failure mode's system level effect and the function definition of every part?
The following picture is the FMEDA calculate tool we used.