This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54561: TPS54561

Part Number: TPS54561


Hi TI,

I have designed a circuit to step down  the input voltage of 48V to 24V with expecting an output current of 3.1A.Could you please verify the circuit to know any issues are there in the circuit. I also have faced an issue in the previous circuit while designing a regulator to step down input  voltage of 48V TO 24 using a AP66300FVBW-13 (Diodes Incorporated). The issue was occurred when  hot swapped the input power connector frequently.so my concern is whether i have to add any protective schemes in the current circuit.