Other Parts Discussed in Thread: TMS570LS3137, TMS570LS1224
Hello,
In the user guide, it is mentioned that connecting the BQ79616s in a daisy-chain stack structure allows them to be controlled by the MCU through the bridge device BQ79616. This will establish a BMS (Battery Management System) system.

There are two different designs to control the number of devices on the right side of the image above:
a) Control with MCU between 3-4 devices.
b) Control with MCU up to 30 devices.
What are the advantages and disadvantages of these two options? When choosing an MCU, what factors should be considered in the given options?