This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Incase if the file is not accessible, please find the problem below
System Inputs
VIN = 16V to 32V
IOUT = 0.2A
VOUT = 12V
The system inputs are fed into WEBENCH designer and the schematic suggested by the designer is
The schematic drawn in simetrix
The output voltage is not stable even though the switching is proper
Could you please support us in identifying the issue ?
https://docs.google.com/spreadsheets/d/1620b7fTfap6h3FqHOqMDAVBq-gXDhlySIxyl8IF3Mv0/edit#gid=0
Hi A.P.
Thank you for designing with the LM5163. Sorry our serve does not allow me to download your google doc file.
Anyway, I am not sure if your transfer of the pspice model to Simplis causes any errors. Could you simulate with TINA, or Pspice, or Pspice for Ti?
Thanks,
Youhao