Other Parts Discussed in Thread: CSD18540Q5B, LM5152EVM-BST
Hello
Please tell me about the simulation model (transient) of LM5152-Q1.
The description of the model's application note includes the following statement.
2. The test bench is set at VIN = 5V, VOUT = 10V, Iout = 5A.
Does this mean that this setting cannot be changed?
For example, is it possible to stably output VIN from 6.5V to 12V, VOUT to 12.5V, and Iout to 9A?
4. The following features are not modeled
a. clock synchronization
b. Clock dithering
c. Switching frequency program by RT.
Enter the desired switching frequency (FSW) in the script window (F11).
Does the fact that this is not modeled mean that synchronization with FPMW mode or external clock is not possible?
Also, although the model does not have an RT pin, does this mean that the corrections will be applied automatically if you input an external clock?
Best regards,
takahashi