Part Number: TPS65987D
Other Parts Discussed in Thread: TPS6598X-CONFIG, TPS55289
Hi team,
My customer designed prototype board using TPS55289RYQR and TPS65987DDH. TPS55289RYQR is controlled by TPS65987DDH via I2C.
SPI Flash(XT25F16BDFIGT) is connected to TPS65987DDH, but it's currently blank.
It would be necessary to generate binary file using TPS6598X-CONFIG for the SPI Flash, but it's not sure how to generate the binary file for below setting.
Would it be possible to provide sample binary file for below condition?
(1)SPI Flash binary data for TPS65987DDH (5V setting, 15V setting) of USB Host setting
(2)SPI Flash binary data for TPS65987DDH (5V setting, 15V setting) of USB Device setting
They simply would like to connect the two prototype boards with a USB Type-C cable, and confirm that they can set 5V → 15V via CC/PD.
TPS65987DDH will not be set ALT.
Best regards,
Shota Mago