Other Parts Discussed in Thread: TLV809
Hello, MCP809 support team
I have three question on MCP809.
- What is POR threshold voltage? Is it 1.0V?
- What is the output type of /RESET pin? Open-drain or Push-Pull?
- When /RESET pin is pulled up to VCC via 100kΩ, Which of #1 and #2 is correct behavior as /RESET pin? As far as I see the Pin Description, I think it looks like /RESET #2.


Regards,
Tamio