This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
TI Team,
Can TPS61378-Q1 support below load/conditions?
Hi Piotr,
TPS61378-Q1 can work in Vin = 3.3V and Vout = 8V, and output 8.2W (Iout = 1.025A).
When RLIM = 20kΩ, the minimum guaranteed maximum output power is around 9.7W. Since the maximum output power is controlled by the peak current limit, the limitation is not so accurate. Again When RLIM = 20kΩ, the range of maximum output power is 9.7W ~ 14W (typ12W).
TPS61378-Q1 has EN pin and power-good pin.
For a short summary, TPS61378-Q1 can meet all the listed requirements. The only concerns is that the limited max output power can't be in 9.5W accurately.
Just let me know if you see any concerns.
Regards
Lei