Other Parts Discussed in Thread: LM5158, LM5156, LM5155
Hi,
I would like to use a TI flyback controller(output power 15W,no external MOSFET required) for a DC-DC flyback converter with 3 outputs, two of them being not isolated(3.3V/2A and 12V/300mA), one of them being isolated(12V/100mA). I want to regulate directly from the non-isolated output(3.3V/2A) without the opto coupler. The total output power is 11.4W. The input voltage range is 16VDC-60VDC.
Thank you so much.