Hello.
After I test the output current limit of TPS768Q1D, I found it was broken. It couldn't operate normally.I set the source voltage 4.3V and current 1A.Then I test the output current .By the way ,I chose resistors vauled 30.1K and 53.6K so that its output voltage value can reach 3.3V. After testing the output current limit, I found it couldn't output 3.3V.
Perhaps there was false in my method. Should I set the source voltage 0V to cater the condition that output voltage is zero?What the right way to test output current limit?
Thanks for you answer.