Dear Expert
Could u hlep to review the sch ,many thanks !
Could u hleo tell me after lowering the two legs, the SS will also discharge internally, right ?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Dear Expert
Could u hlep to review the sch ,many thanks !
Could u hleo tell me after lowering the two legs, the SS will also discharge internally, right ?
Hi,
I will review the schematics and usually such a review needs a bout a week when I will reply to you.
I am not understand your question - what do you mean lowering the two legs? It is better you just indicate which circuit to be controlled like what and what is possible expectation
Dear Hong
Sorry to translate incorrect .
It's means 2PIN put low lever SS pin could be discharge internally .
Any sch review update will be really greatfull .
Hi,
Thanks for the update!
I will review the schematics when comes to this one.
Hi,
Do you mean when pin 2 is low, SS will be discharged internally? If so, yes.
On you schematics:
- suggest remove C89, a typical application COMP does not have such a capacitor.
- Q3 and Q5 do not need R-C snubber (C38, C47, etc) - these can make the performance worse
- The diode in series connected to R64 should be bypassed - where did you see such a diode use?
- U9, pin 6, where is 15VP from?
- Add R-C in parallel with R61 as place holder in case needed
- What is D24 associated circuit function?