Other Parts Discussed in Thread: BQ76942
Hi!
This is a question about the discharge function of the bq77PL900. (SLUS844B–JUNE 2008–REVISED JANUARY 2009, Figure 1. Stand-Alone Mode )
Even if discharge is not intended, if the Pch FET controlling discharge is short-circuited, current may flow to the load via the parasitic diode of the Pch FET controlling charge.
Especially if the current to the load is not at the level to blow the fuse, I think the current will continue to flow.
While the current value can be monitored by the resistance of the sense resistor, if the Pch FET for discharge fails, it seems there is no means to stop the current. However, is there a way to stop the current in such cases?
Thanks!