This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS546C23: questions of datasheet and EVM

Part Number: TPS546C23


Hi team,

I have some question between datasheet and EVM user's guide.

1. In the TPS546C23 datasheet, Slave's FB is connected to BP3, but comp is not connected. On the EVM's slave, FB is connected to COMP. Is there any difference?

2.Do you have a complete EVM schematic? How are RSP/RSN connected? Where are R14/R17 connected?

3. Currently my customer setting register's current fault at 37A but when output current at 18A will trigger OCP when Rshare (ishare pin's resistor) is 0 ohm. Output current at 29A will trigger OCP when Rshare is 10Kohms.Output current at 32A trigger OCP when Rshare is 100Kohms. do you have any idea on this situation?

BR,

Jimmy