Part Number: LMG1020
Hi,
What does the Up to 60 MHz Operation depend on?
What is the limiting factor for this operating parameter? And do you offer similar part that can operate higher than 100MHz?
This thread has been locked.
If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.
Hi VR,
The maximum frequency of the LMG1020 is limited by the PCB layout, choice of FET to drive, and other components like gate resistors. The LMG1020 can theoretically achieve higher operating frequency, but we do not guarantee that it will perform within the characteristics defined in the datasheet.
Thanks,
Rubas
Hi VR,
I'm not familiar with using a gate driver as an XOR gate. Can you share more details a schematic? In general, as long as the absolute max specs are not violated, we can guarantee that the device will work as intended.
Thanks,
Rubas
Hi VR,
If you are talking about the method used in section 8.2.2.2 on the datasheet, then yes that is possible. However, like before, using a frequency higher than 60MHz does not guarantee that the device will perform within the datasheet specs.
Thanks,
Rubas
No problem! Please let me know if there's more questions, otherwise please select the resolved button.
Thanks,
Rubas