This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

Looking for a low speed PWM Controller



Hi,

I need a 30V ,30A, 400Hz PWM output power stage near 100% PWM.

I'm looking for a PWM controller with a frequency of 400Hz.

What I need is a low frequency current mode controller to drive my high side switch, to be able to protect my Hi-side Mos in case of short at the input. I'm working on a buck converter without inductor and capacitor.

Do you have a list of controller with this operating frequency ?

Do you have a better solution to make a high power PWM output ?

Thanks

Alex