This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ2970: BQ297xx is the device comparison table on the data sheet correct?

Part Number: BQ2970


Hi dear people,

Looking to the data sheet, on the device comparison table is said that there should be a device having an UVP-Setting of 2.0 V (last row, by the general BQ297xy data, UVP (V) = 2.0-2.8)

However, I cannot find the device on the table and therefore I am wondering if and where is the typo...

Actually I wanted to use the BQ29706 with OVP = 3.850V and UVP = 2.5V
Could you please confirm that the info on the data sheet corresponds to this version of the IC?

Thanks and  best regards,

Gustavo