Other Parts Discussed in Thread: TPS74901
Hi Team,
Customer report that when the load (electronic load) is set to CC mode 2.7A, the device restarts repeatedly and the peak output current is as high as about 8A. This appears to be due to thermal shutdown being triggered.
Power consumption
(3.3V-1.8V)*2.7A = 4.05W
Expected temperature rise
4.05*49.3(JEDEC) = 199.7℃
4.05*34.9(EVM) = 141.3℃
Can you please help analyze and suggest whether the high inrush peak current is expected? Can it be verified on EVM?
waveform
Regards,
Hailiang