This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

TPS54J060: Bode plot questions

Part Number: TPS54J060

Hi Team,

Customer test the loop of TPS54J060 and have questions on the Bode plot. 

Vin=12V, Vout=1.0V, L=1.5uH, Cout=47uFx3, Rdivider_up=1.1k, Rdivider_down=10k, Cff=NA.

Question: The curve is not smooth, I think they're from the distortion at low and hi freq in the bode instrument. Do you have any comments?

Left : null load;
right: Full load 1.5A.

Regards,
Hailiang