Hey Buck Regulator team,
I have a customer working on a power tree for a new design and we were hoping your team could provide some guidance. Please see a summary of the input/output requirements below in addition to some questions!
We’re attempting to use a flybuck on several designs. Do you have any idea how discontinuous we can run while maintaining stability? All the TI docs and tools say to target 40% ripple (continuous mode), but I’m not sure if that’s controller related or just an arbitrary target based on perceived sweet spot for losses. If it’s controller related, I guess we could increase the load of the non-isolated output as needed. It would be 100% wasted power, but I don’t think we care.
We have 3 output voltage cases to cover. This is a gate drive application with 3 high side windings and 1 for low side. Vin range is approximately 16-20V. Output case 1 is 18V. Output case 2 is 21V. Output case 3 is 25V. These output cases are dependent on the SiC we are using. The total power required is probably around 2-3W.
Does LM5160 with flybuck topology seem appropriate for this?
Is it ok if we choose inductance that is DCM at our typical operating condition? If not, we may have to switch upwards of 1MHz or increase the load on the non-isolated output as needed but would rather not if it isn’t necessary.
Looking forward to your feedback!
Best regards,
Matt Calvo