This thread has been locked.

If you have a related question, please click the "Ask a related question" button in the top right corner. The newly created question will be automatically linked to this question.

BQ25730: Question on application of BQ25730

Part Number: BQ25730


Dear TI team,

I am seeking a load sharing solution using the BQ25730 IC

Primary power source of 12V 6A

Secondary power source of a Rechargeable LiFePO4 of 12V/8Ah Capacity

The System will need 12V/5A to run.

Is the BQ25730 best candidate for this application?

Any suggestions would be greatly appreciated!

Best regards,

Bruno